Hi,
I developed a firmware on top of an example project(From SDK 2.9.0) that works completely fine.
When I try to do the Same with an another existing firmware, It throws Ki2c_busy always right after the first I2C_RTOS_Transfer. The underlying SDK/Drivers are from SDK 2.5.0.
Is It good idea/Preferred to mix the corresponding Drivers new related to I2c with the drivers from old SDK?
已解决! 转到解答。
Hi,
The problem was related with shallow copying a handle that i found out later.
The older drivers works fine.
Thanks a lot for your inputs.
Hi viveknath_thula
Thanks for your interest in the NXP kinetis product, I would like to provide service for you.
To be honest, I suggest you use the newest SDK driver directly, just discard the old SDK2.5.0 version.
Maybe the new SDK version fixed some driver bugs in the old drivers, so you can create the new project based on the newest SDK, then add the other code to your project with new SDK.
Don't mix the old and new driver, as when you find issues, it is difficult to find the root issue, which will be time-consuming. But if you use the new SDK, at least the new SDK project can make it work directly and give you a refernece.
Wish it helps you!
If you still have questions about it, please kindly let me know.
Best Regards,
Kerry