This is all making a lot more sense. You work is much appreciated, I just wish that this kind of work would have been available from the top (NXP) so people like you don't have to create it and people like me don't have to go looking for it.
Just for clarification / understanding. Under the projects Component Manager, Under the Operating System Tab, FreeRTOS is available for slection but... the project seems to already have FreeRTOS in it.
Where is the diconnect in McuXpresso not knowing about freertos? and will this become an issue?
I've never used freertos but I'm taking this as an opportunity to dive in. I just wish I had a bit more streamline way to learn about it. I am feeling pretty lost right now and I'm not sure where to start.
It looks like this is all setup to be a USB Device, Rather than a Host.
Is there a built in way to make the switch or am I going to need to start over with the USB implementation?
Ultimately I need the USB in Host mode for a Keyboard input/ I don't know what is all included in this project so I'm not sure aht I'm looking for to edit.
Getting this off the ground is proving to be quite the hurdle... but I know I'm not the best at this. However I'm determined to get this figured out.
Any references or further info to help would be greatly appreciated.