Measuring clock in KEA-128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Measuring clock in KEA-128

5,478 Views
vigneshbalaji
Senior Contributor I

Hi,

     I want to measure my clock in KEA-128.I am doing this by toggling a GPIO pin in it.I am running my clock at 20Mhz which was the standard example given by NXP(Freescale).But my scope is reading only 583 Khz only.I think I am missing something in it.

I want to know the bus clock per instruction in KEA-128?

The clock per instruction of peripherals?

Can you suggest me a good method to measure the Clock of KEA-128 other than toggling a GPIO?

33 Replies

3,799 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Vignest,

You can check the bus clock on the pin of PTH2 .

First enable the "bus clock output " of this register :

SIM_SOPT0 -> CLKOE

pastedImage_0.png

Hope it helps !


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,799 Views
vigneshbalaji
Senior Contributor I

Hi Alice and David,

                             Both of your answers are working for me.I want to know why normal GPIO toggling won't work.Is it because of number of instructions taken to do it?

Can you please provide any diagram or place where it is mentioned that PTH2 is directly connected to the system clock.Thank you ffor your help.

0 Kudos
Reply

3,797 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNESH BALAJI,

    See you again!

    Actually, about this question, I already answer you in your CASE:

GPIO toggle is using the GPIO module, the GPIO module speed is not as faster as the bus clock.

Besides, if you use the GPIO, it still related to the instuction cycles, the compilier, the optimization function,ect.

All these factors will affect the GPIO toggle speed, you can check the according asm code, you will find the detals. If you still want to use GPIO, you can choose FGPIO, it will faster than the GPIO. Write the code, don't use the while, because while still need a lot of cycles, you can use the FGPIO code one by one directly.

eg.

FGPIOE_PRTOR=0X02;

FGPIOE_PRTOR=0X02;

FGPIOE_PRTOR=0X02;

FGPIOE_PRTOR=0X02;

FGPIOE_PRTOR=0X02;

...

But I suggest you use the method which I told you to test the bus clock:

Configure SIM_SOPT0[CLKOE]=1, SIM_SOPT0[BUSFREF]=0, Bus clock output is enabled on PTH2.

This will output bus clock directly!

Wish it helps you!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,797 Views
vigneshbalaji
Senior Contributor I

Thank you jing,

                        The FTM method was good

0 Kudos
Reply

3,797 Views
kerryzhou
NXP TechSupport
NXP TechSupport

OK, that's very good!

If you still have any question, please let me know!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,797 Views
vigneshbalaji
Senior Contributor I

Hi Jing,

            I am having a problem now.I ran my bus clock at 48 Mhz using the below code change.Now I am not able to flash my code.Can you tell me what went wrong and how to fix it?

SIM_SOPT0 = SIM_SOPT0_CLKOE_MASK;

void Clk_Init()

{

  ICS_C1|=ICS_C1_IRCLKEN_MASK; /* Enable the internal reference clock*/

  while(!(ICS_S & ICS_S_LOCK_MASK));      /* Wait for PLL lock, now running at 40 MHz (1280 * 31.25Khz) */

  ICS_S |= ICS_S_LOCK_MASK ;       /* Clear Loss of lock sticky bit */

}

This was the error message I got.I am using segger to Flash the code.Screenshot (11).png

Screenshot (1).png

0 Kudos
Reply

3,797 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNESH BALAJI,

    Now please follow me to mass erase your TRK-KEA128 at first, besides, you can't use this code:SIM_SOPT0 = SIM_SOPT0_CLKOE_MASK;, this code is not correct.

   Mass erase the TRK-KEA128 process:

1. install the JLINK driver

    After you install the JLINK driver,  you will find the J-Link Commander software.

80.jpg

2. Make sure you are using the JLINK firmware in your TRK-KEA128, from the picture which you give me, I find you already using the JLINK firmware.

The following step is very important!

3, unplug the TRK-KEA128 USB cable in J16, hold on the SW3, don't release the SW3 then plug the USB cable to your PC.

4,don't release the SW3, open J-LINK Commander windows:

81.jpg

You can find the JLINK can find the core now!

5.don't release the SW3, input command in the JLINK Commander windows: unlock kinetis

82.jpg

Waiting the : Timeout while unlocking device   come out

6, release the SW3, input command in the JLINK Commander windows: usb

83.jpg

Until now, your chip is masserased, you can program it again, but take care,modify your code:

SIM_SOPT0 = SIM_SOPT0_CLKOE_MASK;

to

SIM_SOPT0 |= SIM_SOPT0_CLKOE_MASK;

Because if you use the SIM_SOPT0 =, you will clear bit SWDE, this will disable the SWD debug interface, that's why you can't program agan!

Please follow my step, mass erase your chip at first!

Wish it helps you!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,797 Views
vigneshbalaji
Senior Contributor I

Hi Jing,

            I am actually getting this message.I explicitly grounded the reset pin for the holding switch instruction.

I am actually using J-Link STR9 Commander.Is that Fine???

Screenshot (17).png

0 Kudos
Reply

3,797 Views
vigneshbalaji
Senior Contributor I

Hi Jing,

           It is not detecting KEA-128.I went sent that in settings also both by selecting ARM-M0+ and by Manufactureres list(where I selected as SKEAZ-1284 and tried both security and normal one).

Please combine all the 3 replies from me.

0 Kudos
Reply

3,797 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNESH BALAJI,

   I know if you just connect the board, then use the JLINK COMANDER  you will can't find the core, but did you follow my step?

   Hold on the SW3 before you plug the USB cable, and don't release it, just hold on it all the time before you do the mass erase!

    I already use your code, and use my method do the mass erase a lot of times, each time I can successfully mass erase it, and after you mass erase the chip, you can release the SW3.

  Take care, hold on the SW3 before your board is power on, and keep on holding it after you power on and before you successfully mass erased it.

Wish it helps you!

Jingjing

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,797 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNESH BALAJI,

I have not used J-LINK STR9 Commander before, I am not sure whether it works on the kinetis.

  I suggest you install the JLINK driver which I suggest before, then you will find the JLINK COMMANDER

Wish it helps you!

Jingjing

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,797 Views
vigneshbalaji
Senior Contributor I

Hi Jing,

           I checked the voltage at the SWD pin.It is not pulled high.It is at 2 volts.If the SWD is disabled will the reset pin also be disturbed ? I will try by Explicitly pulling it low and then high.

0 Kudos
Reply

3,797 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNGSH BALAJI,

    Please follow my method to mass erase your chip at first, otherwise, you can't program it, because the chip's SWD pin function has been disabled by your code.

Wish it helps you!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,797 Views
vigneshbalaji
Senior Contributor I

Hi Jing,

            In the J-link Driver Link you gave me.I downloaded the Software and Documentation pack.In that I found only J-link STR commander under version 5.10.

Your version shows 5.02 .Should I go back to the older version If so where Can I find them I am trying Hard to Find them.Can you please chaeck out whether the package I downloaded is right?

I have attached the Screenshot of what I downloaded Screenshot (18).png

0 Kudos
Reply

3,797 Views
kerryzhou
NXP TechSupport
NXP TechSupport

See my V5.10g install information:

89.jpg

I still can see the JLINK Commander tool!

Jingjing

0 Kudos
Reply

3,797 Views
kerryzhou
NXP TechSupport
NXP TechSupport

My version is 5.10c, not 5.02, you see the wrong item.

I will try version 5.10g, please wait a moment!

Jingjing

0 Kudos
Reply

3,799 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello VIGNESH,

- How about your code to toggling the GPIO pin ?

- About the bus clock output , please refer to the KEA128RM, the PTH2 pin is the bus clock pin,

pastedImage_0.png

and configure the "CLOKOE" and "BUSREF" to select the value of the pth2 pin out put.

pastedImage_0.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,799 Views
davidsherman
Senior Contributor I

I would suggest using the FlexTimer in PWM mode, and have it toggle one of the outputs. It uses bus clock as the clock source and is much more straightforward than disassembling the source and computing instruction cycles.  Not all instructions use the same number of clock cycles.

3,799 Views
vigneshbalaji
Senior Contributor I

Hi,

    Is there a constrain that we should not run the bus clock at 48Mhz???

I modified my clock like this and found that my controller is not in a flashable state.

Can you tell me what has happened behind this?I am not able to flash my controller after this?

This was my clock code

    SIM_SOPT0 = SIM_SOPT0_CLKOE_MASK;

void Clk_Init()

{

  ICS_C1|=ICS_C1_IRCLKEN_MASK; /* Enable the internal reference clock*/

while(!(ICS_S & ICS_S_LOCK_MASK));

  ICS_S |= ICS_S_LOCK_MASK ;       /* Clear Loss of lock sticky bit */

}

0 Kudos
Reply

3,799 Views
davidsherman
Senior Contributor I

The bus clock cannot run faster than 24MHz.  You will have to change the SIM_CLKDIV register to make sure the bus clock is divided by 2 from the core clock BEFORE you set the ICS for 48MHz.