MQX 4.2, usb_v2 for the K53 - no bsp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX 4.2, usb_v2 for the K53 - no bsp

ソリューションへジャンプ
1,274件の閲覧回数
kfranz
Contributor III

I am porting code that was running on a K64 to a K53. Everything is working except for the USB port. Our code uses usb_v2 but there is no usb_v2 project support for the K53. I am using the IAR EWARM tools. I started with the usb_v2 project for the K64 copied it and edited it for the K53. But, in "C:\Freescale_MQX_4_2\usb_v2\usb_core\device\sources\bsp" there is no bsp for the K53 and the K64 usb_dev_bsp.c breaks when I try to use it on the K53 (I guess that is no surprise).

 

Does anyone have a usb_v2 port for the K53 that uses the IAR EWARM tools?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,258件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

I am very sorry , there is no USB_V2 for K53.  There will be no new features or bugfixes for MQX 4.2. MQX v4.2 is no longer available & superseded by MQX v5.

Please refer to below link for more details.
https://www.nxp.com/design/software/embedded-software/mqx-software-solutions/mqx-v5-software-solutio...

Anyway, you can contact the owner of MQX now, Embedded access , to see if he can provide a solution to you.
http://embedded-access.com/

 

 

Regards

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,259件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

I am very sorry , there is no USB_V2 for K53.  There will be no new features or bugfixes for MQX 4.2. MQX v4.2 is no longer available & superseded by MQX v5.

Please refer to below link for more details.
https://www.nxp.com/design/software/embedded-software/mqx-software-solutions/mqx-v5-software-solutio...

Anyway, you can contact the owner of MQX now, Embedded access , to see if he can provide a solution to you.
http://embedded-access.com/

 

 

Regards

Daniel

0 件の賞賛
返信