MKW30Z Advertise data params

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKW30Z Advertise data params

1,048 次查看
lucianfiran
Contributor V

KW40Z_Connectivity_Software_1.0.1 KSDK_1.3.0 IAR 7.5

https://www.bluetooth.com/specifications/assigned-numbers/generic-access-profile

What additional data should be contained in advertising data as best practice ?
(AdFlags, ServiceList, ClassOfDevice, ManufacturerSpecificData, TxPowerLevel)

gap_types.h
/*! AD Type values as defined by Bluetooth SIG used when defining gapAdStructure_t structures for advertising or scan response data. */
typedef enum gapAdType_tag {
    gAdFlags_c                               = 0x01,    /*!< Defined by the Bluetooth SIG. */
    gAdIncomplete16bitServiceList_c          = 0x02,    /*!< Defined by the Bluetooth SIG. */
    gAdComplete16bitServiceList_c            = 0x03,    /*!< Defined by the Bluetooth SIG. */
    gAdIncomplete32bitServiceList_c          = 0x04,    /*!< Defined by the Bluetooth SIG. */
    gAdComplete32bitServiceList_c            = 0x05,    /*!< Defined by the Bluetooth SIG. */
    gAdIncomplete128bitServiceList_c         = 0x06,    /*!< Defined by the Bluetooth SIG. */
    gAdComplete128bitServiceList_c           = 0x07,    /*!< Defined by the Bluetooth SIG. */
    gAdShortenedLocalName_c                  = 0x08,    /*!< Defined by the Bluetooth SIG. */
    gAdCompleteLocalName_c                   = 0x09,    /*!< Defined by the Bluetooth SIG. */
    gAdTxPowerLevel_c                        = 0x0A,    /*!< Defined by the Bluetooth SIG. */
    gAdClassOfDevice_c                       = 0x0D,    /*!< Defined by the Bluetooth SIG. */
    gAdSimplePairingHashC192_c               = 0x0E,    /*!< Defined by the Bluetooth SIG. */
    gAdSimplePairingRandomizerR192_c         = 0x0F,    /*!< Defined by the Bluetooth SIG. */
    gAdSecurityManagerTkValue_c              = 0x10,    /*!< Defined by the Bluetooth SIG. */
    gAdSecurityManagerOobFlags_c             = 0x11,    /*!< Defined by the Bluetooth SIG. */
    gAdSlaveConnectionIntervalRange_c        = 0x12,    /*!< Defined by the Bluetooth SIG. */
    gAdServiceSolicitationList16bit_c        = 0x14,    /*!< Defined by the Bluetooth SIG. */
    gAdServiceSolicitationList32bit_c        = 0x1F,    /*!< Defined by the Bluetooth SIG. */
    gAdServiceSolicitationList128bit_c       = 0x15,    /*!< Defined by the Bluetooth SIG. */
    gAdServiceData16bit_c                    = 0x16,    /*!< Defined by the Bluetooth SIG. */
    gAdServiceData32bit_c                    = 0x20,    /*!< Defined by the Bluetooth SIG. */
    gAdServiceData128bit_c                   = 0x21,    /*!< Defined by the Bluetooth SIG. */
    gAdPublicTargetAddress_c                 = 0x17,    /*!< Defined by the Bluetooth SIG. */
    gAdRandomTargetAddress_c                 = 0x18,    /*!< Defined by the Bluetooth SIG. */
    gAdAppearance_c                          = 0x19,    /*!< Defined by the Bluetooth SIG. */
    gAdAdvertisingInterval_c                 = 0x1A,    /*!< Defined by the Bluetooth SIG. */
    gAdLeDeviceAddress_c                     = 0x1B,    /*!< Defined by the Bluetooth SIG. */
    gAdLeRole_c                              = 0x1C,    /*!< Defined by the Bluetooth SIG. */
    gAdSimplePairingHashC256_c               = 0x1D,    /*!< Defined by the Bluetooth SIG. */
    gAdSimplePairingRandomizerR256_c         = 0x1E,    /*!< Defined by the Bluetooth SIG. */
    gAd3dInformationData_c                   = 0x3D,    /*!< Defined by the Bluetooth SIG. */
    gAdManufacturerSpecificData_c            = 0xFF     /*!< Defined by the Bluetooth SIG. */
} gapAdType_t;

What is the purpose of Incomplete Service List ?

Should be use to add more 128b UUID's ?

app_config.c
/* Scanning and Advertising Data */
static const uint8_t adData0[1] =  { (gapAdTypeFlags_t)(gLeGeneralDiscoverableMode_c | gBrEdrNotSupported_c) };
static const uint8_t adData1[] = { 0xE0, 0x1C, 0x4B, 0x5E, 0x1E, 0xEB, 0xA1, 0x5C, 0xEE, 0xF4, 0x5E, 0xBA, 0x50, 0x55, 0xFF, 0x01};
static const gapAdStructure_t advScanStruct[3] = {
  {
    .length = NumberOfElements(adData0) + 1,
    .adType = gAdFlags_c,
    .aData = (void *)adData0
  },
  {
    .length = NumberOfElements(adData1) + 1,
    .adType = gAdComplete128bitServiceList_c,
    .aData = (void *)adData1
  },
  {
    .length = 8 + 1,
    .adType = gAdShortenedLocalName_c,
    .aData = "FSL_OTAC"
  }
};

gapAdvertisingData_t gAppAdvertisingData =
{
    NumberOfElements(advScanStruct),
    (void *)advScanStruct
};


There is a way to assert the length of adv data package ?

size  = NumberOfElements(advScanStruct);  assert( size <= LIMIT ) ?
Or compile time check ?
LIMIT should be 31 bytes ?


The value value_device_name should be the same as gAdShortenedLocalName_c aData ?
gatt_db.h
PRIMARY_SERVICE(service_gap, gBleSig_GenericAccessProfile_d)
    CHARACTERISTIC(char_device_name, gBleSig_GapDeviceName_d, (gGattCharPropRead_c) )
        VALUE(value_device_name, gBleSig_GapDeviceName_d, (gPermissionFlagReadable_c), 19, "FSL_BLE_OTAP_CLIENT")
    CHARACTERISTIC(char_appearance, gBleSig_GapAppearance_d, (gGattCharPropRead_c) )
            VALUE(value_appearance, gBleSig_GapAppearance_d, (gPermissionFlagReadable_c), 2, UuidArray(gUnknown_c))
    CHARACTERISTIC(char_ppcp, gBleSig_GapPpcp_d, (gGattCharPropRead_c) )
        VALUE(value_ppcp, gBleSig_GapPpcp_d, (gPermissionFlagReadable_c), 8, 0x0A, 0x00, 0x10, 0x00, 0x64, 0x00, 0xE2, 0x04)

Thank you,
Lucian.

标签 (1)
0 项奖励
回复
0 回复数