MKV44 SDK 2.8.0 missing XBARA Driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MKV44 SDK 2.8.0 missing XBARA Driver

跳至解决方案
2,146 次查看
katha
Contributor II

Hello,

I try to add the XBARA driver to my MKV44 project, but I cant find it in the SDK. In SDK for MK64 2.8.2 it is available. Is there any reason?

Thanks a lot and kind regards

0 项奖励
回复
1 解答
2,136 次查看
Masmiseim
Senior Contributor I

I can not explain why they are missing for the KV44, however they are included in the SDK package for the KV46. This should also work for the KV44. I would give it a try

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,137 次查看
Masmiseim
Senior Contributor I

I can not explain why they are missing for the KV44, however they are included in the SDK package for the KV46. This should also work for the KV44. I would give it a try

0 项奖励
回复
2,113 次查看
katha
Contributor II

Is there a possibility to add it soon?

Whats about the ftm driver? In reference manual it has an extra section besides the eFlexPWM

Regards

0 项奖励
回复