Hello,
we have to use UART1 with 8N2. -> 2 stop bits
Maybe i am blind, but i can't find any µC register for that.
Is it true, that the microcontroller doesn't have this feature?
If yes, is there a work arround?
Andreas
Hi,
Refer to the RM, the uart only supports one stop bit. The data length can be 8 or 9. So you are right. We do not have 2 stop bit feature.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------