MKM34Z256VLL7 controller mmCAU unit, required more information on the letter designations used.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKM34Z256VLL7 controller mmCAU unit, required more information on the letter designations used.

964 次查看
shaiknisar
Contributor I

I'm working with  MKM34Z256VLL7  controller. It processes operations required when processing encryption/decryption algorithm. The support for algorithms is mentioned in 32-bit register maps, denoted with letter designations. I want to know what these letter designations are about. There isn't much information on these letter designations. Can someone help me on these? # MKM34Z256VLL7

标记 (1)
0 项奖励
回复
1 回复

872 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi shaik,

The function of these CAU_CAx register is not fixed. They changed with algorithm. It is not necessary to understand what each register means. Please just refer to the SDK example. It has all the algorithm's demo.

 

Regards,

Jing

0 项奖励
回复