MKM34Z256 Comparator input impedance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MKM34Z256 Comparator input impedance

跳至解决方案
1,875 次查看
petr_uhlir
NXP Employee
NXP Employee

Dear Colleagues,

our customer wants to use MKM34 comparators in their application  And there is question they didn’t find the answer in the documents:

They want to use the three high speed comparator modules in the KM34Z256 to detect an overcurrent as fast as possible. (one for each phase). To connect our external circuit to the comparator input, they must know their input impedance. If the impedance of the comparator inputs is as low as the ADC inputs (some kOhm) than they must add separate impedance converter.
If the input is like a CMOS-Comparator (several MOhm) then the impedance converters are not needed.

Can you tell me the input impedance of the comparator inputs?

Thank you and kind regards,

Petr

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,721 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Petr,

 

I received information from the design team:

 

The answer is impedance <5K ohm after checking with IP owner.

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,722 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Petr,

 

I received information from the design team:

 

The answer is impedance <5K ohm after checking with IP owner.

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,721 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Petr,

I just asked the design team about this parameter. I will let you know as soon as I have any update.

Best regards,

Felipe

0 项奖励
回复