MKM14Z64ACHH5(LGA-44) Which pin should I connect to I2C slave?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKM14Z64ACHH5(LGA-44) Which pin should I connect to I2C slave?

608 Views
bon
Contributor I
Dear customer support,
I am planning to use a I2C slave(SHT31 sensirion attached datacheet) with  MKM14Z64ACHH5(LGA-44).
I have a question about
Which pin should I connect to I2C slave?
I am confused by reading KM Family Reference Manual_MKMxxZxxACxx5RM.
This reference manual says MKM14Z64ACHH5 has one I2C communication interface on page 46 Table 2-2.
But,
The Datasheet(Table 8.2 KM Signal Multiplexing and Pin Assignments) says MKM14Z64ACHH5(LGA-44) has two I2C interfaces below.
Pin No.26 I2C1_SDA
Pin No.27 I2C1_SCL
Pin No.38 I2C0_SCL
Pin No.39 I2C0_SCL
0 Kudos
1 Reply

466 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

The MKM14Z64ACHH5 has two I2C communication interface. But the I2C1 pins(26 27) are default as XTAL and EXTAL function. If you need to use external reference clock or crystal, then you should use I2C0 module.

The I2C0 module(pin 38 39) is recommanded, since pin 32 and 33 is default as SWD interface that you may need to use it.

MKM14Z64ACHH5 i2c.jpg

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos