MKL25Z128 NOR Flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKL25Z128 NOR Flash

736 次查看
mallapuramphani
Contributor I

Hello,

I want to interface NOR flash, with MKL25Z128 on SPI mode.

My query is how much maximum/minimum Memory i can do. 

Thanks & regards

Phani

标记 (1)
0 项奖励
回复
1 回复

660 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Using the SPI mode to connect external SPI Flash, there doesn't with the memory size limitation.

The external SPI Flash memory doesn't add to the KL25 memory map.

Thank you for the attention.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复