MKL25Z - Fresh device programming via USB port

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MKL25Z - Fresh device programming via USB port

跳至解决方案
1,273 次查看
lore
Contributor I

Hello everyone,

Is it possible to flash a bootloader into a fresh new MKL25Z128VLK4 mcu via USB port (without using SWD/JTAG port)? Or I do need to breakout JTAG pins to my custom KL25 board, and buy an external programmer?

My goal is to to set up by custom board as Mass Storage Device so that new binaries can be copied on it, just like the FRDM behavior.

Thanks in advance

Lore

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
1,055 次查看
BlackNight
NXP Employee
NXP Employee

Hi Lore,

the KL25Z has no ROM bootloader (newer Kinetis devices do have this). So you have to use the SWD/JTAG port to program it the first time.

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,056 次查看
BlackNight
NXP Employee
NXP Employee

Hi Lore,

the KL25Z has no ROM bootloader (newer Kinetis devices do have this). So you have to use the SWD/JTAG port to program it the first time.

I hope this helps,

Erich

0 项奖励
回复
1,055 次查看
lore
Contributor I

Hi Erich,

Thanks for your answer, I think you are referring to the supported device table in the KBOOT page. In this case KL27 should be the right choice.

Lore

0 项奖励
回复