MKL05Z32VLC4 (LQFP32) watchdog issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKL05Z32VLC4 (LQFP32) watchdog issue

1,544 Views
ssarathkumar916
Contributor II

Hi,

We are using MKL05Z32VLC4 (LQFP32) in our product. During the production one of our board got failed. While Debugging , we understood that its watchdog reset the micro controller faster than usual.

We are writing 0xc in the SIM_COPC register for initialisation. We are writing SIM_SRVCOP register at every one second interval.

Please help us to solve this issue.

 

Thanks,

Sarathkumar S 

 

0 Kudos
Reply
2 Replies

1,530 Views
nxf58904
NXP Employee
NXP Employee

Hi,

If watch dog reset affect the debugging,we suggest that disable the wdog before debugging.

 

1,505 Views
ssarathkumar916
Contributor II

Hi,

We are using Rowley Cross works for Devopement and rowley cross connect for debugging. We can able to debug the controller without disabling the watchdog. We checked RCM_SRS0 register after reset. It was 0x20 (Reset caused by watchdog timeout).

Thanks,

Sarathkumar S

0 Kudos
Reply