Hi,i'm still in need of help,please
I have a board were a MKL03Z8VFK4 is mounted,i program and debug it with a Multilink Universal tool.
It is a KDS 3.0.0 project based on KSDK 1.3.0 and Processor Expert.
I did'n touch almost nothing of the generated project,excepts an useless attempt in changing heap size that was 0 by default.Watchdog is disabled.Clock is by default Core=4MHz Bus=2MHz.
It programs and after download the debugger stops at the breakpoint at
PE_low_level_init();
If i let it run over without breakpoints in the simple following for(..)loop it runs forever,pausing it in the for loop that is pretty long,if i press the restart button,the one with a green "play "symbol above a yellow arrow,the program,the program runs without stopping anymore at the breakpoint at
PE_low_level_init();
In the sources window i have messages as
No source available for "0x1c00071c"
No source available for "(gdb[1].proc[42000].threadGroup[i1],gdb[1].proc[42000].OSthread[1]).thread[1].frame[0]" .
What does it depends?
Thanks for your time.