From the MKE18F512VLH16 RM I understand there is Error-correcting code (ECC) on Flash and SRAM memories.
For flash, I could not find any register to enable/disable ECC. Is ECC enabled for flash by default?
I could force double bit error in flash by setting FDFD bit in FTFE_FERCNFG and verify that double 
bit fault interrupt flag DFDIF bit in FTFE_FERSTAT is set. I wanted to understand is there any such similar way to force double bit error for SRAM? Under MCM interface in MCM_LMDR register, CF0 field provides capability for ECC Enable Read Check and ECC Enable Write Generation for TCM (couldnt find much documentation on TCM). By setting CF0[0] to 0 can we disable EEWG for SRAM? I have set ERNCR in MCM_LMPECR register to report RAM non correctable error. Can we force ECC non correctable fault in SRAM and verify that ENC field of MCM_LMPEIR set? Also, do MKE18F512VLH16 has any self test capabilities?
 
					
				
		
 FelipeGarcia
		
			FelipeGarcia
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Divya,
The multiple-bit fault is enabled using the FERCNFG[DFDIE] bit. When the multiple-bit error is detected, the FERSTAT[DFDIF] flag is set, and the interrupt request is generated.
Regarding your other questions:
By setting CF0[0] to 0 can we disable EEWG for SRAM?
Yes.
Can we force ECC non correctable fault in SRAM and verify that ENC field of MCM_LMPEIR set?
Yes, but you will need to enable MCM_LMPECR[ERNCR] to enable reporting this error.
MKE18F512VLH16 has any self test capabilities?
Could you please provide more details about this, I don’t know exactly what you mean.
I hope this helps!
Best regards,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
 Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Felipe,
Thank you for the input. I have enabled the ERNCR error reporting and disabled the EEWG by setting CF[0] to 0x02. Written 32 bit data to the SRAM upper and read the data from same address but could not find the ENC field of MCM_LMPEIR set. Please suggest me a way to force ECC fault in SRAM which sets the ENC field of MCM_LMPEIR.
MCM->LMPECR |= MCM_LMPECR_ERNCR_MASK; /* ECC Noncorrectable error */
 MCM->LMDR[1] = MCM_LMDR_CF0(0x2);
*(uint32_t*)0x20000001 = 0xA5A5A5A5;
uint32_t read_sram = *(uint32_t*)0x20000001;
Regards,
Divya
 
					
				
		
 FelipeGarcia
		
			FelipeGarcia
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Divya,
I am sorry for my late reply. I have checked this with internal team. I was told that it is not possible generate RAM ECC error on purpose, because user can't modify the RAM contents without ECC re-calculation.
Sorry for the inconvenience this may cause you.
Best regards,
Felipe