MKE04Z128VLK4 SPI Fan-out

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKE04Z128VLK4 SPI Fan-out

802件の閲覧回数
bon
Contributor I

What is the fanout of MKE04Z128VLK4 SPI port?

How many slaves can be connected to the SPI port?

I would like to connect 8 slaves to the SPI port.

Best regards,

#MKE04Z128VLK4

ラベル(2)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

670件の閲覧回数
bon
Contributor I

Dear Daniel,

Thank you for your reply.

I would like to connect 8 slaves to one SPI port.

I'm worried about fan out by connecting 8 slaves to one port.

A circuit diagram is attached.

The CS pin is simulated with GPIO.

Best regards,

Ryutaro

新規 Microsoft PowerPoint プレゼンテーション.png

0 件の賞賛
返信

670件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

It is OK to connect 8 slaves to one SPI port.

Regards

Daniel

0 件の賞賛
返信

670件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Ryutaro:

MKE04Z128VLK4 contains two SPI modules that support 8-bit data length.

For the limited pin source, only can connect 2 slaves.  If you need to support 8 slaves, you need to use GPIO to simulate CS.

Regards

Daniel

0 件の賞賛
返信