MKE02Z64 default bus clock after POR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MKE02Z64 default bus clock after POR

跳至解决方案
1,026 次查看
guide19
Contributor II

Hi,

what is the default bus clock of the MKE02Z64 device after POR?

BR,

Jozef

0 项奖励
回复
1 解答
876 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jozef Prokopovic,

    Thank you for your question in our community!

    For understanding the bus clock after POR, we need to know which clock modes after POR. When there is a POR, the clock modes goes to FEI(FLL engaged internal).

    The clock route is as follows picture:

KE02ICS.jpg

so the bus clock is calculated following the formula:

fbus=(fIRC*1024)/2.   (1)

About fIRC frequence, if you are not trim it, it the factory value, is 32.768kHz, so the fbus is about 16.77Mhz. If you have trimmed it ,then fIRC frequence is your trim value.but it is between 31.25–39.0625 kHz , then you can calculate it refer to formula (1)。

You can find the details in the reference manual.

I hope it helps you!

Best regards!

Jingjing

在原帖中查看解决方案

0 项奖励
回复
1 回复
877 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jozef Prokopovic,

    Thank you for your question in our community!

    For understanding the bus clock after POR, we need to know which clock modes after POR. When there is a POR, the clock modes goes to FEI(FLL engaged internal).

    The clock route is as follows picture:

KE02ICS.jpg

so the bus clock is calculated following the formula:

fbus=(fIRC*1024)/2.   (1)

About fIRC frequence, if you are not trim it, it the factory value, is 32.768kHz, so the fbus is about 16.77Mhz. If you have trimmed it ,then fIRC frequence is your trim value.but it is between 31.25–39.0625 kHz , then you can calculate it refer to formula (1)。

You can find the details in the reference manual.

I hope it helps you!

Best regards!

Jingjing

0 项奖励
回复