MKE02Z: Accuracy of trimmed Internal Oscillator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKE02Z: Accuracy of trimmed Internal Oscillator

1,857 Views
colin_campbell
Contributor II

Hi NXP,

We are implementing an MKE02Z16VFM4 CPU based design and would like to confirm the accuracy of the trimmed Internal Oscillator as supplied by the Factory.

Our application uses the Internal Reference Clock in FEI Mode with the fixed 1024 Multiplier, to produce a nominal source clock frequency of 32 MHz. Our reading of the Data Sheet (Table 12: Num 9, 11 and 12) and Reference Manual suggests that each MKE02Z16VFM4 device is supplied pre-trimmed by the Factory, thereby allowing the device to meet the IRC accuracy specification of -1/+0.5% over the full temperature range (-40 to +105C), without any further calibration by the end user - is this correct?

Thanks for the guidance - CC

MKE02Z16VFM4 _irc_spec.PNG

Tags (3)
0 Kudos
Reply
4 Replies

1,652 Views
miduo
NXP Employee
NXP Employee

Hello,

The end customer can trim internal reference clock of ICS by their own. You may would like to make reference this post:

https://community.nxp.com/docs/DOC-95356 

0 Kudos
Reply

1,652 Views
colin_campbell
Contributor II

Hi NXP,

Thank you for the confirmation that the nominal Internal Oscillator Frequency can be trimmed by the end user - that makes sense.

The key item we wanted to confirm is our understanding that each MKE02Z16VFM4 device is supplied pre-trimmed by the Factory to a nominal Internal Oscillator Frequency of 31.25 kHz, which will have an accuracy specification of -1/+0.5% over the full temperature range (-40 to +105C), without any further calibration by the end user - is this correct?

Thanks for the additional guidance - CC

0 Kudos
Reply

1,652 Views
miduo
NXP Employee
NXP Employee

Sorry for the late response. Yes, correctly!

0 Kudos
Reply

1,652 Views
colin_campbell
Contributor II

Hi NXP,

 

Thank you for the confirmation on the accuracy of the trimmed Internal Oscillator as supplied by the Factory - that makes sense.

 

Many thanks - CC

0 Kudos
Reply