In the data sheet it says that SRAM size is 256KB , but in the reference manual section 3.5.3.1 SRAM is 192KB for MK64FX512VLQ12 CPU.
Which information is correct?
Data Sheet:
http://www.nxp.com/assets/documents/data/en/data-sheets/K64P144M120SF5.pdf
Reference Manual:
http://www.nxp.com/assets/documents/data/en/reference-manuals/K64P144M120SF5RM.pdf
解決済! 解決策の投稿を見る。
Hi,
MK64FX512VLQ12 has 256KB SRAM, the datasheet list the correct SRAM memory size.
I will forward Kinetis product team about K64 reference manual table 2-11 with incorrect SRAM size of MK64FX512VLQ12.
Sorry for that may bring any inconvenience to you.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for you help .
Hi,
MK64FX512VLQ12 has 256KB SRAM, the datasheet list the correct SRAM memory size.
I will forward Kinetis product team about K64 reference manual table 2-11 with incorrect SRAM size of MK64FX512VLQ12.
Sorry for that may bring any inconvenience to you.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
It looks like it has 256KB of SRAM. I've just tried your suggestion and it worked. I was able to access 0x2002000 - 0x20030000 address range, with no hard faults.
I guess there is an error in the reference manual .
The linker script file that comes with latest SDK2.2 (generated with SDK builder)for this CPU also limits RAM size to 192KB.
MEMORY
{
m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000400
m_flash_config (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010
m_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x0007FBF0
m_data (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00010000
m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00020000
}
Is linker script also incorrect? I'm wondering if it's save to increase m_data_2 memory area, to get all 256KB?
Alex
This is quite a strange situation - I haven't heard of such a 'serious' error in a user manual before, nor that the reference code follows the error. Nor that the user's manual is still inaccurate after more that 3 years, even after it was reported in the other post in its very latest revision 6 months ago....
Possibly the FX512 parts are rarely used (?) although they are popular for the Teensy 3.5
If you physically have 256k of SRAM you can of course change the length of m_data_2 to 0x00030000
Regards
Mark
http://www.utasker.com/kinetis/FRDM-K64F.html
http://www.utasker.com/kinetis/TWR-K64F120M.html
http://www.utasker.com/kinetis/TEENSY_3.5.html
Hi Alex
Very good question!
One of the two is obviously wrong, but I don't know which.
if you have the chip in question see whether you can access SRAM at 0x20020000. If it hard faults it has 192k, if it doesn't it has 256k.
Regards
Mark