MK64FX512VLL12 demo board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK64FX512VLL12 demo board

363 Views
alexxchen
Contributor I

Is there any demo board with MK64FX512VLL12 on the board available?

0 Kudos
1 Reply

289 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello alex chen,

      MK64FX512VLL12 can refer to the FRDM-K64F120M board:

FRDM-K64F|Freedom Development Platform|Kinetis MCUs|NXP 

  This board is using the MK64FN1M0VLL12 which is the same package as MK64FX512VLL12.

   If you want to get the same chip, I think you can replace the on board MK64FN1M0VLL12 with your MK64FX512VLL12. These two chips are the same package.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos