MK64 default output at reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MK64 default output at reset

跳至解决方案
1,465 次查看
roymessinger
Contributor V

What is the default state of the outputs of the cobtroller immidiately after reset?

Do i need to put pull up/pull down on board?Regarding inputs, do i need to place pull up/pull down on inputs (or outputs) not used?

I've looked in the data sheet but probabely missed it.

Any help will do.

Thanks

0 项奖励
回复
1 解答
1,312 次查看
egoodii
Senior Contributor III

The 'reset state' of all control registers is called out in the Reference Manual, including the 'pin mux' table, but the general statement is: 'reset state is the safest possible for any possible interconnect'.  That is, analog-in-capable pins will default to said analog-in mode, and digital pins will default to input, most with 'no pull'.

So yes, by-and-large anything you need to have as a 'known state' during/just-after reset will need your own external pull-resistors.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,312 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Roy,

Some special function pins need take care. For exmaple: Reset_b\ NMI_b\ VREF_OUT\ JTAG_TMS

I recommend you read the "Chapter 2 General System Setup (Hardware Considerations)" of KQRUG.

General System Setup (Hardware Considerations).png

Best Regards,

Robin

0 项奖励
回复
1,313 次查看
egoodii
Senior Contributor III

The 'reset state' of all control registers is called out in the Reference Manual, including the 'pin mux' table, but the general statement is: 'reset state is the safest possible for any possible interconnect'.  That is, analog-in-capable pins will default to said analog-in mode, and digital pins will default to input, most with 'no pull'.

So yes, by-and-large anything you need to have as a 'known state' during/just-after reset will need your own external pull-resistors.

0 项奖励
回复