MK64 USB+emmc 模拟U-disk,拷出数据速度

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK64 USB+emmc 模拟U-disk,拷出数据速度

Jump to solution
1,392 Views
OneByte
Contributor II

哈喽,大家好,在使用MK64 芯片,用更改SDK中的USB +emmc 模拟成U-disk,发现拷入和拷出数据速度只有500k,有哪些方式可优化?请教一下大家。

注释:

emmc的Vccq 电压3.3v ,4bit,尝试更改full-speed和speed-high等不明显。

0 Kudos
Reply
1 Solution
1,268 Views
OneByte
Contributor II

i get it ,USB of MK64 only support full_speed or low_speed ,it is not supporting high speed .the fast speed of full_speed is 12Mbit/s,so we can do nothing for it.

View solution in original post

0 Kudos
Reply
4 Replies
1,269 Views
OneByte
Contributor II

i get it ,USB of MK64 only support full_speed or low_speed ,it is not supporting high speed .the fast speed of full_speed is 12Mbit/s,so we can do nothing for it.

0 Kudos
Reply
1,366 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Can you please put  your question in English?

0 Kudos
Reply
1,297 Views
OneByte
Contributor II
usb-project of sdk use SD-card,but i change sd to emmc.
Vccq of emmc pull high to 3.3v,high speed of emmc should be connceted to 1.8V(Does this have an impact

?)
0 Kudos
Reply
1,300 Views
OneByte
Contributor II
How to improve USB copy speed by simulating u-disk using MK64 USB MSC SDK
0 Kudos
Reply