MK60DN512ZVLQ10 and FNET 2.1.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK60DN512ZVLQ10 and FNET 2.1.1

1,138 次查看
Arun_bel
Contributor I

I have created a project for MK60DN512ZVLQ10 using FNET 2.1.1 example shell demo application.

But the shell demo app is created for twr- mk60n512 board having MK60DN512VMD100 processor(BGA package).

So I have changed my processor settings and default UART settings.

Now UART is working fine but in Hyperterminal I am getting Link Status: unconnected .

Is there any changes to be done in any file if processor of same family I am using, particularly Pin change requirements.

Thanks and regards

Arun

标签 (1)
0 项奖励
回复
2 回复数

994 次查看
tusharm
Contributor III

Hello Arun,

    

    Check the jumper connection i.e J2 and J3 u keep it for 50Mhz and J12 in RMII mode then execute your programs...If ur board is of 120Mhz i.e MK60F120M then use K70 example code...Or else better u down;load the latest FNET2.5...

Regards,

Tushar M

0 项奖励
回复

994 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi Arun,

  Those packages (144 BGA and 144LQFP) will have the same pinout, so no pin changes are needed.

  Are you trying to run this code on a new custom board? Or are you just changing the software and still trying to run on a TWR-K60N512 board?

-Anthony

0 项奖励
回复