MK60 SPI master doesn't receive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK60 SPI master doesn't receive

1,335 Views
ednasalazar
Contributor II

Hi,

I have a problem with my SPI.

After analysing spi transaction using keil ulink pro debugger and I saw that information sent by SPI slave is not detected.

This is SPI configuration:

void SPI_Init(void) {

/*------------------------------------------------------------------------------

port SPI  configuration

*------------------------------------------------------------------------------*/

      

      SIM->SCGC5 |= SIM_SCGC5_PORTD_MASK;    /* enable clock for PORTB */

     SIM->SCGC3 |= SIM_SCGC3_SPI2_MASK;     /* enable clock for SPI2 */

     // Assign SPI signals to the port pins

     PORTD->PCR[11] &= PORT_PCR_MUX_MASK;

      PORTD->PCR[11] |= PORT_PCR_MUX(2) ; // SPI2 CS

  PORTD->PCR[12] &= PORT_PCR_MUX_MASK;

      PORTD->PCR[12] |= PORT_PCR_MUX(2) ; // SPI2 SCLK

  PORTD->PCR[13] &= PORT_PCR_MUX_MASK;

      PORTD->PCR[13] |= PORT_PCR_MUX(2) ; // SPI2 MOSI

  PORTD->PCR[14] &= PORT_PCR_MUX_MASK;

      PORTD->PCR[14] |= PORT_PCR_MUX(2) ; // SPI2 MISO

/*------------------------------------------------------------------------------

SPI register configuration (MCR Register, CTAR Register, SR Register)

*------------------------------------------------------------------------------*/

     //  Configuration

     SPI2->MCR = SPI_MCR_HALT_MASK;   // halt SPI before SPI setting psSPI->MCR = SPI_MCR_HALT_MASK

     SPI2->MCR &= ~SPI_MCR_MDIS_MASK; // enable module

      SPI2->MCR |= SPI_MCR_MSTR_MASK;   // master mode enabled

      SPI2->MCR |= SPI_MCR_PCSIS(1)    // inactive state of CS signal is high

           | SPI_MCR_DCONF(0)

                | SPI_MCR_DIS_TXF_MASK // disable TX FIFO

      | SPI_MCR_DIS_RXF_MASK; // Disable RX FIFO

  SPI2->MCR |= SPI_MCR_ROOE_MASK; 

      // Setting the SPI protocol in order to match requirements of motor driver                                             

      SPI2->CTAR[0] = SPI_CTAR_PCSSCK(2)  // PCS to SCK Delay Prescaler = 3

                      | SPI_CTAR_CSSCK(3) // PCS to SCK Delay Scaler = 4

                      | SPI_CTAR_PBR(1)   // Baud Rate Prescaler = 2

                      | SPI_CTAR_PASC(3)  // After SCK Delay Prescaler = 5

                      | SPI_CTAR_DT(2)    // Delay After Transfer Scaler

                      | SPI_CTAR_BR(4)    // Baud Rate Scaler = 512

     | SPI_CTAR_ASC(3)   // After SCK Delay Scaler

  | SPI_CTAR_CPHA_MASK

                      | SPI_CTAR_PDT(1)   // Delay after Transfer Prescaler = 7

                      | SPI_CTAR_CPOL_MASK  // clock polarity - inactive state of SCK is high

                      | SPI_CTAR_FMSZ(7) ;    // 9-bit transfer block              

 

       SPI2->SR =    SPI_SR_TCF_MASK           // clear transfert complet flag

  | SPI_SR_EOQF_MASK   // clear end of queue flag

  | SPI_SR_TFUF_MASK   // clear transmit FIFO Fill Flag

  | SPI_SR_TFFF_MASK   // clear transfert complet flag

  | SPI_SR_RFOF_MASK   // clear receive FIFO Overflow Flag

  |SPI_SR_RFDF_MASK;   // clear receive FIFO Drain Flag

      SPI2->RSER = (uint32_t)0x00UL;        // clear DMA interruptions  

      SPI2->MCR &= ~SPI_MCR_HALT_MASK;     // starts DSPI transfers

}

/*************************************************************************

* Function Name: SPI_Send

* Parameters: sending command

*

* Return: received status data

*

* Description: SPI send data handler uint8_t

*

*************************************************************************/

void Send_SPI (SPI_Type *psSPI, uint8_t SPI_data) {

psSPI->PUSHR = SPI_PUSHR_TXDATA(SPI_data) | SPI_PUSHR_PCS(1) ;

while (!((psSPI->SR >> SPI_SR_TCF_SHIFT) & 1)){}; //wait till transmission completes

psSPI->SR |= SPI_SR_TCF_MASK; // clear complete flag 

} /* vSPI_Send */

uint8_t Receive_SPI (SPI_Type *psSPI) {

   while (!(psSPI->SR & SPI_SR_RFDF_MASK));

   return (psSPI->POPR);

} /* uchSPI_Receive */

This is my main.c :

#include "MK60N512MD100.h"

#include "spi.h"

/*----------------------------------------------------------------------------

  MAIN function

*----------------------------------------------------------------------------*/

int main (void) {

  uint8_t x,y;

  SPI_Init();  

   while(1) {

    Send_SPI(SPI2,0xD0);

  x=Receive_SPI(SPI2);

    Send_SPI(SPI2,0x00);

  x=Receive_SPI(SPI2);

  Send_SPI(SPI2,0x00);

   y=Receive_SPI(SPI2);

  }

 

}

When I see SR register of SPI2, I realize that the flag RFDF is clear when the folloging part is executed:

psSPI->SR |= SPI_SR_TCF_MASK;


Thanks very much

Labels (1)
Tags (3)
2 Replies

775 Views
ednasalazar
Contributor II

Thanks

0 Kudos

775 Views
jeremyzhou
NXP Employee
NXP Employee

Hi enna salazar,

I'd like to highly recommend that you should get to understand the communication protocol of the slave device totally through review its datasheet.

I've attached a demo of TWR-K60D100 board about SPI communicate with external flash chips AT26DF081A and I think it help you to establish the connection between the Master and Slave correctly.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------