MK22FX512 FlexCan init problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK22FX512 FlexCan init problem

1,099 次查看
pauvilanova
Contributor III

Hi,

I'm trying to work with the flexcan module of my mk22 using the MCUxpresso drivers provided by nxp, but when I try to initialize the flexcan it gets stuck on the following while:

static inline void FLEXCAN_Enable(CAN_Type *base, bool enable)
{
    if (enable)
    {
        base->MCR &= ~CAN_MCR_MDIS_MASK;
        /* Wait FlexCAN exit from low-power mode. */
        while (base->MCR & CAN_MCR_LPMACK_MASK)
        {
        }...

When enabling CAN, it waits until the lowpowermodule is off, but this bit is never 0. How could that be?

I had CAN working on the KDS so i went to check in there if the driver checks that bit, but it doesn't, enabling can on the kds driver just changes MDIS bit without waiting the lpm to set off.

My mcuxpresso initialization is the following:

    flexcan_config_t flexcanConfig;
    FLEXCAN_GetDefaultConfig(&flexcanConfig);
    FLEXCAN_Init(FLEXCAN0, &flexcanConfig, 8000000UL);

Thanks.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

871 次查看
mjbcswitzerland
Specialist V

Hi

The order of writing clock settings is important - and it will not leave disabled mode if not respected and in freeze mode.
This is the solution from the uTasker project as reference:

    ulCanCtrValue = fnOptimalCAN_clock(pars->usMode, pars->ulSpeed);
    ptrCAN_control->CAN_CTRL1 = (CLK_SRC_PERIPH_CLK & ulCanCtrValue);    // select the clock source while the module is in disable mode
                                                                         // note that the crystal can be used and has better jitter performance than the PLL
    ptrCAN_control->CAN_MCR &= ~CAN_MDIS;                                // move from disabled to freeze mode (un-synchronised to the CAN bus)
    while ((ptrCAN_control->CAN_MCR & CAN_LPMACK) != 0) {                // wait for CAN controller to leave disabled mode
    }
    ptrCAN_control->CAN_CTRL1 = ulCanCtrValue;                           // write the clock setting

Regards

Mark

CAN:
Document: http://www.utasker.com/docs/uTasker/uTaskerCAN.PDF
Video: https://www.youtube.com/watch?v=Ha8cv_XEvco


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html