MK22FN : VREGIN pin is powered when MCU VDD is off.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK22FN : VREGIN pin is powered when MCU VDD is off.

Jump to solution
1,128 Views
koichisakagami
Contributor II

Dear community,

We have been developing our product with MK22FN1M0AVMC12.

We worry about a situation as follows.

The VREGIN pin is connected to VBUS(5v) with USB connector.
When 5v is applied to the  VREGIN pin, the MCU 3.3v voltage is not applied to VDD pin yet.

[Question]
    Does such a situation have any problem for MK22 ?
    For example,
    does it decrease the lifetime of MK22 ?

Best Regards,
    Koichi Sakagami

Labels (2)
0 Kudos
Reply
1 Solution
792 Views
jeremyzhou
NXP Employee
NXP Employee

Hi  Koichi Sakagami,

According to reference manual, the USB regulator should be put into STANDBY mode when the chip is in Stop mode.

When the MCU is not powered by the VDD which is almost equal to the MCU enters the low power mode.

So I'd highly recommend that you should eliminate the put the USB cable to a USB host while the MCU is not powered.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
793 Views
jeremyzhou
NXP Employee
NXP Employee

Hi  Koichi Sakagami,

According to reference manual, the USB regulator should be put into STANDBY mode when the chip is in Stop mode.

When the MCU is not powered by the VDD which is almost equal to the MCU enters the low power mode.

So I'd highly recommend that you should eliminate the put the USB cable to a USB host while the MCU is not powered.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
792 Views
koichisakagami
Contributor II

Dear Ping san,

Thank you for your answer.

I got it.

Best Regards,

Koichi Sakagami

0 Kudos
Reply