MK22DX256VMC5 VOUT33 output not good when VREGIN changes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK22DX256VMC5 VOUT33 output not good when VREGIN changes

3,169 次查看
huijiejiang
Contributor I

We are using the internal regulator, and VOUT33 output voltage(+3.3V on the schematic) rise to 3.8V when there is an fast voltage dip on VREGIN("+5V" on the sch, "+5Vout" in the graph), see below for the sch and graph.

We guess that is because of the PSRR, but we cannot find the PSRR parameter in the datasheet...

What is the root cause and how can we improve the performance?

connection.PNG

tek00001.pngtek00002.png

标签 (1)
标记 (1)
0 项奖励
回复
6 回复数

2,955 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you use USB, you have to use internal regulator to provide power for internal USB transceiver. In the case, you can connect VREGIN to 5V, connect the VOUT33 pin to a 2.2uF capacitor, connect the VDD pins to external 3.3V power supply, you can get 3.3V power supply with an external LDO or general regulator such as LM1117-3.3V device.

Hope it can help you

BR

'XiangJun Rong

0 项奖励
回复

2,955 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, HuiJie,

If you use external LDO to provide power for the K22,  internal regulator is NOT used, in the case, when USB is not used in the application, it is recommended to
connect VREGOUT and VREG_INx together and tie to ground
through a 10kΩ resistor. Do not tie directly to ground, as this
causes a latch-up risk. For systems where only one of the
VREG_INx pins is ever used, it is also recommended to
connect the two VREG_INx pins together.

BR

Xiangjun rong

0 项奖励
回复

2,954 次查看
huijiejiang
Contributor I

Hi Xiangjun,

Thanks for the reply.

But we will use the USB function, and if we use the external LDO, how to treat with VREGIN and VOUT3.3?

0 项奖励
回复

2,955 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, HuJie,

The VDD power supply ranges from -0.3V to 3.8V, so I think it is okay.

As you know that the VOUT33 is  the internal regulator output, the internal regulator inputs 5V, it is not related to the PSRR(power supply rejection rate). how about  using different capacitor on the VOUT33 pin, which can ranges from 1.76uF to 8.16uF.

Hope it can help you

BR

Xiangjun Rong

0 项奖励
回复

2,955 次查看
huijiejiang
Contributor I

Hi Xiangjun,

Thanks for your quickly reply.

I have tried your suggestion to add additional capacitors to C9 and made it as 4.4uf, 6.6uf..., and did the test with the same method, but there was no improvement.

Based on the test, the fluctuation of the VOUT3.3 is reduced when the voltage dip is reduced and seams not so related to the capacitor, which meets the requirement of the datasheet.

Here is the question,

1) Do you have the PSRR of the regulator?

2) Is there any additional requirement for the VREGIN that related with VOUT3.3? 

0 项奖励
回复

2,955 次查看
huijiejiang
Contributor I

Hi Xiangjun,

Is there any update?

regarding the internal regulator,

We design the MCU as a USB device, if we use an external LDO, how to treat the VREGIN and VOUT3.3?

Do we MUST to, as the below picture,

1) connect VREGIN to VBUS

2) add Cstab to VOUT3.3(2.2uf? can that capacitor be used a smaller value one?)

3) connect VDD to external LDO output

Untitled.png

Can we ONLY use the external LDO and just leave away(just float the VREGIN and VOUT3.3) the internal regulator?

0 项奖励
回复