MK22 Uses as USB host and connects USB HUB IC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK22 Uses as USB host and connects USB HUB IC

1,122 Views
lukegu
Contributor I

Dear ,

      My customer will plan to use MK22FX512VLL12 as the USB Host. And use the USB HUB IC -- USB2512 -- to extend the USB connection, the USB device includes USB HID,USB Mouse , etc . Could you kindly help me to check this issue and give me some demo for this ?I mean , some demo code or successful application ?

      Appreciated a lot !

     Have a great day!

0 Kudos
Reply
1 Reply

969 Views
isaacavila
NXP Employee
NXP Employee

Hello Luke,

How are you? Hope you are fine! KSDK 2.0 has support for MK22FX512VLL12 device. You can use USB examples for TWR-K21F120M board which is compatible with K22FX512VLL12.

K22 support.jpg

There are several USB Host examples for different classes  such as HID, MSD, CDC, etc. You can locate them at: <SDK_2.0_MK22FX512xxx12>\boards\twrk21f120m\usb_examples.

Also, in KSDK 2.0 documentation, it is stated that some external HUBs (not IC HUBs as your customer wants to use) were tested on these examples:

USB HUBs.jpg

But basically there should be no problem when using this IC HUB (Customer should implement the serial communication between K22 and IC HUB through serial interface).

I hope this helps!

Regards,

Isaac

0 Kudos
Reply