MK20DX128VFM5 IC question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK20DX128VFM5 IC question

1,121 次查看
shinezen
Contributor III

i design circuit board , i use the MK20DX128VFM5  IC ,the power is ok

1.why  IC pin 19(reset pin) have clock 18khz?

2.the IC initial firmware is open sda2.1??

3.i have a SEGGER JLINK (JTAG),so can i use that progamming MK20DX128VFM5?

4.can i  programming MK20DX128VFM5 IC by usb port

thanks for your help

标签 (2)
0 项奖励
回复
2 回复数

978 次查看
rastislav_pavlanin
NXP Employee
NXP Employee

Hi,

not clear what kind of board is used in your design. Is it our FRDM board? or your based design.

answers:

1. looks like your K20 device is in periodic reset e.g. caused by core lock up due to blank flash content.

2. well, if it is our FRDM board you use then OpenSDA K20 device contains OpenSDA bootloader application firmware pre-programmed. However, if it is K20 you have bought then the device is blank (empty flash content, all 0xFFFFFFFF).

3. yes, you can use jLink to program the device

4. ? if FRDM board used then you need to use SDA JTAG connector (10 pins 50mils micro header), we usually do not populate it on FRDM boards (you need to buy it and populate). You cannot use USB on FRDM board to program K20 OpenSDA device.

0 项奖励
回复

978 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Could you let us know which board you are using? Thanks.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复