MK20DN512VLQ10: What is output mode of EZP_Q in EzPort mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK20DN512VLQ10: What is output mode of EZP_Q in EzPort mode?

783 次查看
isaotakashima
Contributor IV

Currently we are building a flash programming equipements using EzPort for the MK20DN512VLQ10.

If we add external 10k ohm pull down resistor to the EZP_Q pin of the MK20DN512VLQ10, EZP_Q cannot output high level.

If we add external 10k ohm pull up resistor or no external resistor to EZP_Q pin, EZP_Q can output high level.

Why does this phenomenon occur?

What is output mode of EZP_Q in EzPort mode?

Please reply as soon as possible.

Best regards,

Takashima

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

669 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Takashima,

When the EZP_CS signal is high, the EZP_Q is tri-stated, external pull up or down determine the logic of the pin.

when the EZP_CS signal is low, the EZP_Q is driven on the falling edge of EZP_CK, in the case, the EZP_Q pin is push-pull driven.

Have you transferred data by clearing the EZP_CS signal?

Hope it can help you

BR

Xiangjun Rong

0 项奖励
回复