MK10 family: doubt on ADC resolution for single ended channels

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK10 family: doubt on ADC resolution for single ended channels

Jump to solution
1,177 Views
gabrielemarocco
Contributor I

I have a doubt regarding the resolution of ADC single ended channels of MK10 microcontrollers: can I achieve a 16 bits conversion result on single ended ADC channels?

On page 36 of K10 Sub-Family Data Sheet  I have read that 16 bits accuracy can be achieved only on differential channels (ADCX_DP0, ADCX_DM0)

On page 576 of K10 Sub-Family Reference Manual I have read that ADCx_CFG1 can be set to achieve a 16 bits single ended conversion

I need to clarify about this issue in order to choose properly the MCU

Regards, Gabriele

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
858 Views
pavel_krenek
NXP Employee
NXP Employee

Hi Gabriele,

Yes, you can use single ended channel input and achieve accuracy 16 bit on Kinetis K10.

Regards,

Pavel

View solution in original post

0 Kudos
Reply
4 Replies
859 Views
pavel_krenek
NXP Employee
NXP Employee

Hi Gabriele,

Yes, you can use single ended channel input and achieve accuracy 16 bit on Kinetis K10.

Regards,

Pavel

0 Kudos
Reply
858 Views
gabrielemarocco
Contributor I

Just another question: is it possible to achieve the 16 bit accuracy on all the ADC inputs or only on ADCx_DP0, ADCx_DM0?

Thanks, Gabriele

0 Kudos
Reply
858 Views
ozgabai
Contributor I

I have the same question,

is it possible to achieve the 16 bit accuracy on all the ADC inputs or only on ADCx_DP0 ???

Is it possible to achieve 16 bit resolution using the ADC of the MK10DN32VFM5  chip ?

0 Kudos
Reply
858 Views
pavel_krenek
NXP Employee
NXP Employee

• Yes, it is possible. All single ended inputs of ADC can be used with 16 bit resolution.

• Output modes:

     differential 16-bit, 13-bit, 11-bit and 9-bit modes

    single-ended 16-bit, 12-bit, 10-bit and 8-bit modes     

0 Kudos
Reply