MED-EKG demo in the TWR-K53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MED-EKG demo in the TWR-K53

Jump to solution
3,755 Views
luizcamilo
Contributor I

I can not make the software run on a machine Medical_GUI 64bits.

Following is the error:

C:\Freescale\Medical GUI>java -jar medical_gui_v2.2.jar

Exception in thread "AWT-EventQueue-0" java.lang.NoClassDefFoundError: gnu/io/Co

mmPortIdentifier

        at java.lang.Class.getDeclaredMethods0(Native Method)

        at java.lang.Class.privateGetDeclaredMethods(Class.java:2451)

        at java.lang.Class.getDeclaredMethod(Class.java:1954)

        at java.awt.Component.isCoalesceEventsOverriden(Component.java:6190)

        at java.awt.Component.access$500(Component.java:188)

        at java.awt.Component$3.run(Component.java:6144)

        at java.awt.Component$3.run(Component.java:6142)

        at java.security.AccessController.doPrivileged(Native Method)

        at java.awt.Component.checkCoalescing(Component.java:6141)

        at java.awt.Component.<init>(Component.java:6110)

        at java.awt.Container.<init>(Container.java:276)

        at java.awt.Window.<init>(Window.java:437)

        at java.awt.Window.<init>(Window.java:594)

        at java.awt.Dialog.<init>(Dialog.java:665)

        at java.awt.Dialog.<init>(Dialog.java:409)

        at javax.swing.JDialog.<init>(JDialog.java:271)

        at Medical.PortChooser.<init>(PortChooser.java:99)

        at Medical.MedicalCommander.<init>(MedicalCommander.java:65)

        at Medical.MedicalControl.<init>(MedicalControl.java:38)

        at Medical.MedicalControl$1.run(MedicalControl.java:62)

        at java.awt.event.InvocationEvent.dispatch(InvocationEvent.java:251)

        at java.awt.EventQueue.dispatchEventImpl(EventQueue.java:727)

        at java.awt.EventQueue.access$200(EventQueue.java:103)

        at java.awt.EventQueue$3.run(EventQueue.java:688)

        at java.awt.EventQueue$3.run(EventQueue.java:686)

        at java.security.AccessController.doPrivileged(Native Method)

        at java.security.ProtectionDomain$1.doIntersectionPrivilege(ProtectionDo

main.java:76)

        at java.awt.EventQueue.dispatchEvent(EventQueue.java:697)

        at java.awt.EventDispatchThread.pumpOneEventForFilters(EventDispatchThre

ad.java:242)

        at java.awt.EventDispatchThread.pumpEventsForFilter(EventDispatchThread.

java:161)

        at java.awt.EventDispatchThread.pumpEventsForHierarchy(EventDispatchThre

ad.java:150)

        at java.awt.EventDispatchThread.pumpEvents(EventDispatchThread.java:146)

        at java.awt.EventDispatchThread.pumpEvents(EventDispatchThread.java:138)

        at java.awt.EventDispatchThread.run(EventDispatchThread.java:91)

Caused by: java.lang.ClassNotFoundException: gnu.io.CommPortIdentifier

        at java.net.URLClassLoader$1.run(URLClassLoader.java:366)

        at java.net.URLClassLoader$1.run(URLClassLoader.java:355)

        at java.security.AccessController.doPrivileged(Native Method)

        at java.net.URLClassLoader.findClass(URLClassLoader.java:354)

        at java.lang.ClassLoader.loadClass(ClassLoader.java:423)

        at sun.misc.Launcher$AppClassLoader.loadClass(Launcher.java:308)

        at java.lang.ClassLoader.loadClass(ClassLoader.java:356)

        ... 34 more

C:\Freescale\Medical GUI>

0 Kudos
Reply
1 Solution
3,398 Views
CarlosCasillas
NXP Employee
NXP Employee

Hello Luiz,

 

Have you ensured that you computer has 64-bit OS and that you have downloaded and installed Java JDK for 64-bit? The launched GUI installer should also match with the OS and Java versions.

Regarding last MED-EKG projects, they are included on the ZIP file of application note AN4323, at the followinglink:

http://www.freescale.com/files/analog/doc/app_note/AN4323SW.zip

 

Hope this information will be useful for you.

Best regards!

/Carlos

View solution in original post

0 Kudos
Reply
6 Replies
3,394 Views
CarlosCasillas
NXP Employee
NXP Employee

Hello Luiz,

 

Have you installed the Java JDK that corresponds to your operating system before installing the Medical GUI? Detailed steps for proper installation of the Medical GUI on 32 and 64 bits systems are included on the Readme.pdf document that comes with the installer on the same ZIP file. (I have attached this document to this post).

 

If you have installed the Medical GUI without having Java, please uninstall the Medical GUI, then, install the proper Java version, and then, install again the Medical GUI.

 

Hope this information will be useful for you.

Best regards!

/Carlos

0 Kudos
Reply
3,394 Views
luizcamilo
Contributor I

I managed  proceed with the installation, but now is being presented a new error message.

RXTX Version mismatch

JAR version = RXTX-2.2pre2

native lib Version = RXTX-2.2-200081207 cloudhopper Buid rxtx.cloudhopper.net

Can you help me?

Best regarsds!

Luiz

0 Kudos
Reply
3,399 Views
CarlosCasillas
NXP Employee
NXP Employee

Hello Luiz,

 

Have you ensured that you computer has 64-bit OS and that you have downloaded and installed Java JDK for 64-bit? The launched GUI installer should also match with the OS and Java versions.

Regarding last MED-EKG projects, they are included on the ZIP file of application note AN4323, at the followinglink:

http://www.freescale.com/files/analog/doc/app_note/AN4323SW.zip

 

Hope this information will be useful for you.

Best regards!

/Carlos

0 Kudos
Reply
3,394 Views
luizcamilo
Contributor I

Hi,

Thank you Carlos.

Best regards

Luiz

0 Kudos
Reply
3,394 Views
luizcamilo
Contributor I

Hello Carlos.

I have other question, you have a link to project of EKG, I did the download of USB_CDC.eww, but not is the correct.

Can you help me?

Best regarsds!

Luiz

0 Kudos
Reply
3,394 Views
luizcamilo
Contributor I

Hello Carlos.

Thank you for your attention and your time.

I've done this procedure, but had no success.

Best regarsds!

Luiz

0 Kudos
Reply