MCUXpresso IDE support for MK60 F120 MHz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE support for MK60 F120 MHz

807 Views
henrynguyen
Contributor IV

Hello,

The MK60 F120 MHz is supported in KDS.  Is it also supported in MCUXpresso IDE?

it seems to support the MK60 D100 version, but not F120 version.

can you please let us know if there is any future plan to support F120 version?

Thanks,

Henry

0 Kudos
2 Replies

691 Views
mjbcswitzerland
Specialist V

Hi

All devices [incl. K60FN120] are supported in the uTasker project (also available as open source - see link below) which can be used with KDS or MCUXpresso or most other IDEs.
- with integrated TCP/IP, USB, FAT, etc.


Regards

Mark

Complete Kinetis solutions for professional needs, training and support: http://www.utasker.com/kinetis.html

Kinetis K60:
- http://www.utasker.com/kinetis/TWR-K60N512.html
- http://www.utasker.com/kinetis/TWR-K60D100M.html
- http://www.utasker.com/kinetis/TWR-K60F120M.html
- http://www.utasker.com/kinetis/ELZET80_NET-KBED.html
- http://www.utasker.com/kinetis/ELZET80_NET-K60.html

uTasker: supporting >1'000 registered Kinetis users get products faster and cheaper to market

Request Free emergency remote desk-top consulting at http://www.utasker.com/services.html

Open Source version at https://github.com/uTasker/uTasker-Kinetis

uTasker for small, fast code and reliable products: https://community.nxp.com/thread/512558

0 Kudos

691 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Henry:

Unfortunately there is no plan to support MK60F120M in MCUXpresso SDK now.

For K60f120,  you can use bare metal or MQX  for development.

TWR-K60F120M|Tower System Board|Kinetis MCUs|NXP 

pastedImage_1.png

Regards

Daniel

0 Kudos