MCU initialization for K20 series

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCU initialization for K20 series

跳至解决方案
2,519 次查看
evgenik
Contributor IV

Hi.

 

I worked with CW 10.2 IDE. I received from Freescale example boards for K20 but Processor Expert haven't initialization package for K20 MCU. Where I can download update for Processor Expert or Code example for K20 MCU series initialization?

 

Thanks.

Evgeni Kosakovski.

R&D Engineer

0 项奖励
回复
1 解答
1,810 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

I have verified it in the CW V10.2 final version and I have not encountered a problem with selection of K20 MCU in 64 and 32 pin packages.

It seems that the problem was originally caused by providing incomplete ID of the selected MCU. TWR-K20D50M means that the user has 50 MHz variant of the MCU, so the user must select a MCU from the "K20D (50 MHz) Family" group.

 

After correct MCU selection in project wizard, the requested pin variant will be available, for details please see the attached screen-shots.

 

best regards
Vojtech Filip
Processor Expert Support Team

 

 

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,810 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

are you using the final 10.2 (or the beta?).

At least my final 10.2 shows Processor Expert support for K20D and K20F.

 

BK

0 项奖励
回复
1,810 次查看
evgenik
Contributor IV

I correct my question.

We are develop project with Freescale K20 MCU with 64 and 32 pins, but in CW 10.2 Processor Expert haven’t these configurations. Are you have any updates for CW 10.2 or MCU initialization examples for these packages?

 

Evgeni.

0 项奖励
回复
1,810 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

hmm, I see now your point. I have the PK20X128VLH (64pin) on the TWR-K20D50M board.

But Processor Expert only shows the MX20DX128ZVLQ10 package :smileysad:.

 

BK

0 项奖励
回复
1,811 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

I have verified it in the CW V10.2 final version and I have not encountered a problem with selection of K20 MCU in 64 and 32 pin packages.

It seems that the problem was originally caused by providing incomplete ID of the selected MCU. TWR-K20D50M means that the user has 50 MHz variant of the MCU, so the user must select a MCU from the "K20D (50 MHz) Family" group.

 

After correct MCU selection in project wizard, the requested pin variant will be available, for details please see the attached screen-shots.

 

best regards
Vojtech Filip
Processor Expert Support Team

 

 

0 项奖励
回复
1,810 次查看
evgenik
Contributor IV

This is work in the CW 10.2 final version.

 

Thanks.

0 项奖励
回复