Low power mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Low power mode

5,738 次查看
punithb
Contributor I

I am using KEAZN64M2 controller in my custom board. I just want to put my controller in sleep mode.

How can i do that?.

0 项奖励
回复
12 回复数

4,475 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi punith B,

  Here are some driver code enter low power for your reference:

void PMC_Init(PMC_Type *pPMC, PMC_ConfigType *pPMC_Config)

{

    pPMC->SPMSC1 = pPMC_Config->sCtrlstatus.byte;

    pPMC->SPMSC2 = pPMC_Config->sDetectVoltSelect.byte;        

}

void PMC_SetMode(PMC_Type *pPMC,uint8_t u8PmcMode)

{

    switch(u8PmcMode & 0x3)

    {

        case PmcModeRun:   

            break;

        case PmcModeWait:

            /* Clear the SLEEPDEEP bit to make sure we go into WAIT (sleep) mode instead

             * of deep sleep.

             */

            SCB->SCR &= ~SCB_SCR_SLEEPDEEP_Msk;

            /* Not using KEIL's uVision, so use the standard assembly command */

            asm("WFI");

            break;

        case PmcModeStop4:

            /* enable LVD in stop mode */

            pPMC->SPMSC1 |= (PMC_SPMSC1_LVDE_MASK | PMC_SPMSC1_LVDSE_MASK);

            /* Set the SLEEPDEEP bit to enable deep sleep mode (STOP) */

            SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;

            /* Not using KEIL's uVision, so use the standard assembly command */

            asm("WFI");

            break;

        case PmcModeStop3:

            /* disable LVD in stop mode */

            pPMC->SPMSC1 &= ~(PMC_SPMSC1_LVDE_MASK | PMC_SPMSC1_LVDRE_MASK | PMC_SPMSC1_LVDSE_MASK);

            /* Set the SLEEPDEEP bit to enable deep sleep mode (STOP) */

            SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;

            /* Not using KEIL's uVision, so use the standard assembly command */

            asm("WFI");

            break;

        default:

            break;

    }

}

More details, you can refer to FRDM_KEA64_PMC sample code in this link:

SDK Software Drivers for KEAZ128_KEAZ64 using S32DS

Wish it helps you!


Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,475 次查看
punithb
Contributor I

Thank you for support. and could you please let me know fallowing query.

How to put S9S12GA240 micro controller in sleep mode?. What is cpu current

taking in sleep and run mode?

On Fri, Jul 29, 2016 at 8:22 AM, kerryzhou <admin@community.freescale.com>

0 项奖励
回复

4,475 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi punith,

    I am the kinetis engineer, not the 16bit mcu engineer.

  So, if you have the 16bit mcu question, please go to this link, and create a new question:

S12 / MagniV Microcontrollers


Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,475 次查看
punithb
Contributor I

Hi Jingjing

Ok I will ask in same. In run mode my board is taking 53mA. even if i put

in sleep mode the current is same.

Here how i did.

ICS->C1 &=~ICS_C1_IRCLKEN_MASK; /* Disable the internal reference clock*/

PMC->SPMSC1 = 0x80;

PMC->SPMSC2 = 0x00;

PMC->SPMSC1 &= ~PMC_SPMSC1_LVWIE_MASK;

/* disable LVD in stop mode */

PMC->SPMSC1 &= ~(PMC_SPMSC1_LVDE_MASK | PMC_SPMSC1_LVDRE_MASK |

PMC_SPMSC1_LVDSE_MASK);

/* Set the SLEEPDEEP bit to enable deep sleep mode (STOP) */

SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;

/* Not using KEIL's uVision, so use the standard assembly command */

__WFI;

while(1);

Please let me know what is the problem?.

On Fri, Jul 29, 2016 at 1:01 PM, kerryzhou <admin@community.freescale.com>

0 项奖励
回复

4,476 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi punith,

    What the test point you are measure the current in your board? You should make sure the test point just measure the KEA chip's currect, not include other external chip, you can post the schematic which shows your power measurement testpoint.

    Before you enter the stop mode, what the internal module your are enabled? 53mA is high to MCU if you didn't enable any other peripheral  according to the datasheet.

    Did you enable the interrupt before enter sleep mode?  interrupt will wake up the sleep mode, we need to know whether the chip is waked up immediately after entering the sleep mode.

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,476 次查看
punithb
Contributor I

Hi Jingjing,

Now I am able to generate the RTC interrupt which is working fine. Thank

you for your support. Could you please let me know what is current will

take by RTC in both wake and sleep mode?. In my board i am using internal

clock as bus clock.

0 项奖励
回复

4,476 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi punith B,

    For the detail RTC consumption, you need to test it on you side, because the datasheet normally just give the mcu consumption, and it didn't give the module consumption in detail situation.

  Our datasheet just give the data in the stop mode with LPO clock:

  RTC adder causes IDD to increase typically by less than 1 μA; RTC clock source is 1 kHz LPO clock.

  So, if you want to use the internal bus clock, you can test it on your board.


Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,476 次查看
punithb
Contributor I

Is it possible to wake the controller from GPIO interrupt method instead of

RTC timer interrupt?.

On Thu, Aug 4, 2016 at 4:24 PM, kerryzhou <admin@community.freescale.com>

0 项奖励
回复

4,476 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi punith,

  From the reference manual:

pastedImage_0.png

  You can get that the interrupt can wake up the sleep mode, so you can use GPIO interrupt to wake up the sleep mode.


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,476 次查看
punithb
Contributor I

Thank you for your support? Could you please let me know what all GPIO i

can use as GPIO interrupt for KEA64 controller to wake from sleep?.

On Wed, Aug 10, 2016 at 12:08 PM, kerryzhou <admin@community.freescale.com>

0 项奖励
回复

4,476 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Punith,

    KEA64 don't have the GPIO interrupt, so you need to use IRQ or KBI interrupt.

  IRQ is assigned to pin PTAB5 by default.

  KBI pin can be PTA0,PTA1,PTA2,PTA3, PTB0-PTB3.

Wish it helps you!

Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,475 次查看
punithb
Contributor I

Hi Jingjing,

I have used fallowing in my code for RTC in my code to comes out of sleep

mode but RTC interrupt not at all executing.

In main

/* Initialize RTC */

RTC_ConfigType RTC_Config=;

RTC_Config.u16ModuloValue = 3;

RTC_Config.bInterruptEn = 1; /* Enable interrupt */

RTC_Config.bClockSource = RTC_CLKSRC_1KHZ;/* Clock source is 1khz */

RTC_Config.bClockPrescaler = RTC_CLK_PRESCALER_1000; /* Prescaler is

100 */

RTC_SetCallback(RTC_Task);

RTC_Init(&RTC_Config); /* Initialization of RTC */

in interrupt

void RTC_Task(void)

{

/* toggle BLUE LED */

//OUTPUT_TOGGLE(PTE,PTE7); /* Toggle on BLUE LED *

//printf("\nRTC routine.\n"); /* Print Message */

}

I am using internal clock as main clock in my code which is 25MHZ.

could you please let me know why RTC interrupt is not working?.

Regards

Punith

0 项奖励
回复