Lockup on Reset Pin in VLLS2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Lockup on Reset Pin in VLLS2

1,286 次查看
leifzars
Contributor IV

When in VLLS2 and the reset pin is hit, the System Reset Status Register reads a Lockup. This is using a Kinetis MK24FN1M  (1N8B3J).

Previously using the MK20DN512 (5N22D) this did not happen, I would get a PIN reset code.

Anyone experience this, or know a work around?

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,167 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Leif,

I don't quite know what you mean 'lockup'. I made a test on my TWR-K24F120M. I download the example power_mode_switch by keil. In Project->option->debug->setting->Reset, I select 'reset pin'. Then I let the chip into VLLS2. Then I press the RESET button on KEIL. The SRS register will be 0x41.

Then in Project->option->debug->setting->Reset, I select 'Core and peripherals'. And do same operate as before, the SRS register read as 0x1.

So I didn't see any problem. Can you give more detail about your question?

Regards

Jing

0 项奖励
回复

1,167 次查看
leifzars
Contributor IV

In manual 6.2.2.9 Lockup reset (LOCKUP).

I must have something miss configured with my setup. Would you think the issue is on boot?

Any thoughts?

0 项奖励
回复