Locked kinetis

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Locked kinetis

2,707 次查看
FlyChou
Contributor I

Is there anybody debug Kinetis with J-LINK?

I got a problem.J-Link Commander print as below:

SEGGER J-Link Commander V4.40a ('?' for help)Compiled Dec 16 2011 20:52:58DLL version V4.40a, compiled Dec 16 2011 20:52:42Firmware: J-Link ARM V8 compiled Dec  6 2011 18:57:44Hardware: V8.00S/N: 20100214Feature(s): RDI,FlashDL,FlashBP,JFlash,GDBFullVTarget = 3.287VInfo: TotalIRLen = 4, IRPrint = 0x01Info: ARM AP[0]: 0x24770011, AHB-APInfo: ARM AP[1]: 0x001C0000, JTAG-AP****** Error: No APB-AP found.No devices found on JTAG chain. Trying to find device on SWD.Info: Found SWD-DP with ID 0x2BA01477Info:   FPUnit: 0 code (BP) slots and 0 literal slotsNo device found on SWD.Did not find any core.Info: TotalIRLen = 4, IRPrint = 0x01Info: ARM AP[0]: 0x24770011, AHB-APInfo: ARM AP[1]: 0x001C0000, JTAG-AP****** Error: No APB-AP found.No devices found on JTAG chain. Trying to find device on SWD.Info: Found SWD-DP with ID 0x2BA01477Info:   FPUnit: 0 code (BP) slots and 0 literal slotsNo device found on SWD.Did not find any core.

 I have tried the command "unlock kinetis", but does not work.

J-Link>unlock kinetisFound SWD-DP with ID 0x2BA01477Unlocking device...Timeout while unlocking device.J-Link>unlock kinetisFound SWD-DP with ID 0x2BA01477Unlocking device...Timeout while unlocking device.

 I am wondering if my board is OK.  Any suggestion for Me?

0 项奖励
回复
4 回复数

1,523 次查看
zm92011
Contributor I

Did you find a solution?

0 项奖励
回复

1,523 次查看
rhyttr
Contributor I

When use SWD interface, cause there is no reset signal to JLINK

 

Solution:

Open jlink. Exe command tool, when hint as follows, must pull low CPU reset pin


Pull low reset pin, click "yes", will be prompted to find Cortex-the M4, Run command "unlock kinetis" then unlock successful!


0 项奖励
回复

1,523 次查看
jame
Contributor I

i have the same problem,and i try "unlock kinetis","erase_all_pin.jlk",but it still can't be solved.why?

0 项奖励
回复

1,523 次查看
FlyChou
Contributor I

Is there anybody can help me ?

Or just give me some suggestion ... Thx

0 项奖励
回复