Lock up RESET in kinetis K61during Application is running.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lock up RESET in kinetis K61during Application is running.

875 Views
virendrapatel
Contributor III

Hello,..

We have customized  hardware board based on kinetis K61Fx512.Our system is having bootloader and application program which runs on RTXC OS.

We have observe that the our application runs successfully for 5 to 10 min and then the board is reseted, this issue is observe in 2 boards only. When we checked for the reason for reset, we came to know that it is due to LOCKUP RESET.

We don't know how to investigate the root cause of LOCKUP RESET during application running.

Can anybody help us to debug this issue? or what are the possible reason which cause the LOCKUP reset?

Thanks,

Virendra

0 Kudos
Reply
0 Replies