Lderror in KEA series microcontroller using S32ds IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lderror in KEA series microcontroller using S32ds IDE

5,233 Views
rkavinash03
Contributor I

I am using KEA series microcontroller, when I try to enable freemaster, It shows SRAM overflow. I couldn't resolve this error. attached the image for reference. Please help me in resolving this issue.

Labels (1)
0 Kudos
Reply
4 Replies

5,228 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Have you tried Light version (achieving smaller RAM/flash footprint)?

Light version (achieving smaller RAM flash footprint).png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,222 Views
rkavinash03
Contributor I

Dear sir,

               I still got that error even after changing to light version. Attached image for reference.

I changed FMSTR_REC_OWNBUFF to 1, There are NO errors.

0 Kudos
Reply

5,216 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

It is recommended that you ask questions on the FreeMASTER forum, where there are FreeMASTER experts who can provide more help.

0 Kudos
Reply

5,213 Views
rkavinash03
Contributor I

Ok sir. Thank you

 

0 Kudos
Reply