LPTMR in the KL04 chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPTMR in the KL04 chip

Jump to solution
2,457 Views
vinkar
Contributor III

Hello Friends,

I have a mysterious behavior in my KL04 chip. My aim is to simple start running the LPTMR as a free running timer. At an event occurence I see the LPTMR0_CNR and calculate ,based on my clk to the LPTMR, the duration. Now, as I am using it as a free running timer, I presume, it does not need LPTMR0_CMR as I am not comparing with anything. Also, I am not using any interrupts, so I kept the LPTMR0_CMR = 0;

The code is below -

#include "derivative.h" /* include peripheral declarations */

int main(void)

{

    int count;

    uint16_t countTemp = 0;

   // asm(" CPSIE i");

   

   

    MCG_C1 |= 0x02;

    MCG_C2 |= 0x01;

    SIM_SOPT1 = 0;      

    SIM_SCGC5 |= (SIM_SCGC5_LPTMR_MASK | SIM_SCGC5_PORTB_MASK);//PORTC_PCR1 |= PORT_PCR_MUX(1);//select RTC_CLKIN function

   

    PORTB_PCR3 |= 0x00000100;    // alternative pin mux selection //

    GPIOB_PDDR |= 0x00000008;    // pin direction //   

    PORTB_PCR4 |= 0x00000100;    // alternative pin mux selection //

    GPIOB_PDDR |= 0x00000010;    // pin direction //        

   

   

    MCG_SC = 0x40;

    SIM_SCGC5|=SIM_SCGC5_LPTMR_MASK;

    /* Reset LPTMR settings */

    SIM_SOPT1 = 0;   

   

    SIM_SCGC5 |= (SIM_SCGC5_LPTMR_MASK | SIM_SCGC5_PORTB_MASK);//PORTC_PCR1 |= PORT_PCR_MUX(1);//select RTC_CLKIN function

    LPTMR0_CSR=0;  

    //LPTMR0_CSR |= 0x00000040;

    LPTMR0_CMR = 0;

   

   

    GPIOB_PTOR |= (1 << 3);

    GPIOB_PTOR |= (1 << 4);  

   

    LPTMR0_PSR |= 0x04;

   

    GPIOB_PTOR |= (1 << 3);

    GPIOB_PTOR |= (1 << 4);  

     /* Start the timer */ 

    LPTMR0_CSR |= LPTMR_CSR_TEN_MASK;

     /* Wait for counter to reach compare value */

   

    asm("nop");

   

   

    while(1){               

        asm("nop");

        asm("nop");

        asm("nop");

        asm("nop");

        LPTMR0_CNR = 45;

        count = LPTMR0_CNR;

        if(count >7000){

          LPTMR0_CSR &= ~LPTMR_CSR_TEN_MASK;

          LPTMR0_CSR |= 0x00000040;

          LPTMR0_CNR = 45;

        count = LPTMR0_CNR;

        LPTMR0_CSR |= LPTMR_CSR_TEN_MASK;

      }

       

    }      

}

I am first writing a junk value (in this case 45) to LPTMR0_CNR and then reading it. Always the value in LPTMR0_CNR is '0'.

But, then I made LPTMR0_CMR = 8000;

Then did the same code. This time around, the value of LPTMR_CNR went upto 8000 or so and then a roll over. So, despite all this there is

a comparison and a rollover causes a reset of LPTMR0_CNR. Y So !!!!!!!

Vinod

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,175 Views
DavidS
NXP Employee
NXP Employee

Hi Vinod,

I was able to get the attached code to run using CW10.6.+ PE.  The main.c #define can be changed to run baremetal code or PE code.

Regards,

David

View solution in original post

0 Kudos
Reply
5 Replies
2,175 Views
yasuhikokoumoto
Senior Contributor I

Hello vinod,

after all. your purpose is to use LPTMR as 16 bit free run counter ?

As David says, the problem was you had forgotten to set TFC bit of TMPR0_CSR?

Please let us know your purpose.

Best regards,

Yasuhiko Koumoto.

0 Kudos
Reply
2,175 Views
vinkar
Contributor III

Hello Sir,

Yes I found that out and is now working. Thank you Mr Koumoto and Mr Seymour for all the help.

VInod

0 Kudos
Reply
2,176 Views
DavidS
NXP Employee
NXP Employee

Hi Vinod,

I was able to get the attached code to run using CW10.6.+ PE.  The main.c #define can be changed to run baremetal code or PE code.

Regards,

David

0 Kudos
Reply
2,175 Views
yasuhikokoumoto
Senior Contributor I

Hello vinod,

thank you for your correct answer at another my post.

You are right. First, I could not understand your comment.

Do you claim for not keeping LPTMR0_CMR 0?

However, LPTMR0_CMR=0 indicates the LPTMR0_CNR is always reset.

Anyway, what inconveniences do you have if LPTMR0_CMR is set 0xffff (i.e. the maximum value)?

Please tell me the purpose of your post.

Best regards.

Yasuhiko Koumoto.

0 Kudos
Reply
2,175 Views
yasuhikokoumoto
Senior Contributor I

Hello vinod,

I tried the same scenario and found a strange behavior.

That is, LPTMR0_CNR is always showing 0.

However, the compare interrupt caused as normally.

What happened?

I am afraid there are some setting to show LPTMR0_CNR value.

Best regards,

Yasuhiko Koumoto.

0 Kudos
Reply