Hello,
I have tried to use the touch screen from the TWR-LCD connected to the primary elevator to my TWR-K60F120. Although I have succeeded in using the LCD to display a screen, the touch screen doesn't seem to work.
So I have tried to load the "tchres" demo project, using the "tchres" touch screen driver from MQX, and I noticed this line :
#if (BSP_TWR_K70F120M || BSP_TWR_K60F120M)
#error This application can not be supported on twrk70f120m and twrk60f120m boards (Used ADC have not gpio alternative).
My question is the following : can I use the touch screen in any way directly from the TWR-K60F120 connected to a LCD screen or is it not possible at all because of the reason mentioned above ?
Thank you for your answer !
Camille
已解决! 转到解答。
Hi Camille,
Yes and No. You can't connect directly the TWR-K60F120 to TWR-LCD because of the explained reason. But you could make a rework using TWR-PROTO
Remove R6, R7, R8, R9. On K60 120Mhz
TWR-PROTO - just only for demos with K70/K60. There must be add 4 wires to interconnect:
B27 - B59
B28 - B70
B29 - B58
B30 - B19
Regards,
Luis
Hi Camille,
Yes and No. You can't connect directly the TWR-K60F120 to TWR-LCD because of the explained reason. But you could make a rework using TWR-PROTO
Remove R6, R7, R8, R9. On K60 120Mhz
TWR-PROTO - just only for demos with K70/K60. There must be add 4 wires to interconnect:
B27 - B59
B28 - B70
B29 - B58
B30 - B19
Regards,
Luis