Kv30F64电流采样问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kv30F64电流采样问题

Jump to solution
689 Views
yaoXin
Contributor II

 

KV30F64的ADC外设,支持对差分输入和单端输入的模拟量采样,我的项目中先通过ADC0,ADC1采集两路差分输入,再通过ADC0采集一路单端输入,并且保持循环采样,循环周期为62.5us。ADC模块时钟为12MHZ(48MHZ进行4分频),不开启long sample time采样,分辨率都设置为16位,也不开启硬件平均功能。

  ADC0的差分输入连接到管脚ADC0_DP1,ADC0_DM1,ADC1的差分输入连接到管脚ADC1_DP1,ADC1_DM1,ADC0的单端输入连接到管脚ADC0_SE23。

    把单端信号通过100K电阻连接到Gnd上,外部只保留100PF电容,每次在对它进行采样时,发现信号上会出现接近200mv的电压跳变。检查ADC配置未发现明显异常,这种情况可能是什么原因?

yaoXin_0-1657875428459.png

yaoXin_1-1657875485797.png

 

 

Labels (1)
0 Kudos
1 Solution
661 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi yaoXin,

100K电阻值太大了。 数据手册Kinetis KV30: 100MHz Cortex-M4F 64/128KB Flash 32-64pin

的Table 23. 16-bit ADC operating conditions 章节中可以看到RADIN Input series resistance 最大才5K

可以看一下这篇:ADC外部RC电路电阻和电容选取计算方法 https://mp.weixin.qq.com/s/l5afihUlRecSW0o7BOYJbA

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
662 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi yaoXin,

100K电阻值太大了。 数据手册Kinetis KV30: 100MHz Cortex-M4F 64/128KB Flash 32-64pin

的Table 23. 16-bit ADC operating conditions 章节中可以看到RADIN Input series resistance 最大才5K

可以看一下这篇:ADC外部RC电路电阻和电容选取计算方法 https://mp.weixin.qq.com/s/l5afihUlRecSW0o7BOYJbA

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos