Kinetis MK20DX256VLK10 bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Kinetis MK20DX256VLK10 bootloader

跳至解决方案
1,370 次查看
francescoferrar
Contributor III

Hi

I need to update the FW for my board on the field.

Can you recommend a bootloader for MK20DX256VLK10 micro among the many possibilities that Freescale offers?

The time to implement the solution is few,  this is why a quick fix would help me.

Best Regards

Francesco

0 项奖励
回复
1 解答
1,264 次查看
francescoferrar
Contributor III

Hi Jingjing

I resolved. My board is connected to the host via usb cable.

I ported freedom_bootloader for K64F from FSL_Kinetis_Bootloader_1_2_0

thanks anyway for the reply

Francesco

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,264 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Francesco Ferraro,

      Do you want to use the UART bootloader?

     If yes, you can refer to the application note and it's sample code.

    The application note is AN2295:

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN2295.pdf?fsrch=1&sr=1&pageNum=1

    The according sample code is AN2295SW:

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN2295SW.zip

Wish it helps you!

If you still have question, please let me know!

Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,265 次查看
francescoferrar
Contributor III

Hi Jingjing

I resolved. My board is connected to the host via usb cable.

I ported freedom_bootloader for K64F from FSL_Kinetis_Bootloader_1_2_0

thanks anyway for the reply

Francesco

0 项奖励
回复
1,264 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Francesco,

   That's very good to hear you solved the question.

   If the post answers your question, please click the Correct Answer button. Thank you!

Best Regards,

Jingjing

0 项奖励
回复