Kinetis M Series (KM1x and KM3x) 24 bit ADC Performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis M Series (KM1x and KM3x) 24 bit ADC Performance

Jump to solution
2,141 Views
bvenus
Contributor I

The current datasheet for the KM series only outlines the 16 bit ADC specifications.

What is the 24 bit ADC specifications, specifically SINAD and ENOB?

0 Kudos
Reply
1 Solution
1,729 Views
apanecatl
Senior Contributor II

You can find the 24-bit specs in the following chapter: 6.4.4.2 ΣΔ ADC Standalone specifications of the devices datasheet, the document can be downloaded from the following link:

http://cache.freescale.com/files/32bit/doc/data_sheet/MKMxxZxxACxx5.pdf

View solution in original post

0 Kudos
Reply
3 Replies
1,730 Views
apanecatl
Senior Contributor II

You can find the 24-bit specs in the following chapter: 6.4.4.2 ΣΔ ADC Standalone specifications of the devices datasheet, the document can be downloaded from the following link:

http://cache.freescale.com/files/32bit/doc/data_sheet/MKMxxZxxACxx5.pdf

0 Kudos
Reply
1,729 Views
rabbitz
Contributor I

If the MCU run at 50Mhz clock and sampling with 24 bit resolution, do you know how fast can it sampling?

0 Kudos
Reply
1,729 Views
MarMi
NXP Employee
NXP Employee

The SD ADC conversion rate depends on the modulator clock (fmclk) and selected oversampling ratio (OSR). Datasheet parameters of the SD ADC (for normal operation) are specified for fmclk=6.144MHz and OSR=2048, where such configuration results in 3 ksps output sample. You can go down with OSR to 64, which will increase output sample rate to 96 ksps still providing 24-bit result but with lesser noise free bits (~ -2.8 bits).

0 Kudos
Reply