Kinetis K70 and 8-bit NAND Flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Kinetis K70 and 8-bit NAND Flash

跳至解决方案
2,441 次查看
andreyvarsegov
Contributor I

Hi,

I can not find the documentation for the connection diagram via NFC and 8-bit NAND Flash chip.

How to connect the data bus ?  In 8-bit mode used NFC_D0-NFC_D7 or NFC_D8-NFC_D15?

NFC_D0 - NAND_D0

...

NFC_D7 - NAND_D7

or

NFC_D8 - NAND_D0

...

NFC_D15 - NAND_D7

Best regards, Andrey.

标签 (1)
标记 (5)
0 项奖励
回复
1 解答
2,072 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Andrey

Sorry, I think as Flexbus by mistake.You should connect low data bus. Please reference attached picture.8-bit NFC.jpg

Best Regards

Paul

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,072 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Andrey

You can connect to FB_D0 - FB_D7.

0 项奖励
回复
2,072 次查看
andreyvarsegov
Contributor I

Thank you for quick answer, but you sure to FB_D0 - FB_D7 ? May be NFC_DATA0 - NFC_DATA7, because at TWR-K70F120M-SCH.pdf  16-bit NAND Flash connected to NFC_DATA0-DATA15, not to FB_D0-D15.

Best regards, Andrey.

0 项奖励
回复
2,072 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Andrey,

In NFC 8-bit mode, please connect  NFC_D0-NFC_D7 with external 8-bit NAND Flash device.

Wish it helps.

2,072 次查看
andreyvarsegov
Contributor I

Hi Hui_Ma,

Thank you very match!

Best regards, Andrey.

0 项奖励
回复
2,073 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Andrey

Sorry, I think as Flexbus by mistake.You should connect low data bus. Please reference attached picture.8-bit NFC.jpg

Best Regards

Paul

0 项奖励
回复