Hi,
I want to interface a 32bits data wide SDRAM to a Kinetis K66 144 Pins.
The Datasheet is really confusing about the data line, I can only see that D31-D16 is available on the package, but the manual refers to SDRAM_D [31:0] (Table 35-2)
Are the remaining Data I/O from Flexbus?
Also I cannot correlate the example in AN5095 to the latest K65 user guide, pins arrangements must have changed.
Am I missing something obvious?
Thanks.