Kinetis K61 Erratta #5952 - LLWU from LLS/VLLS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K61 Erratta #5952 - LLWU from LLS/VLLS

Jump to solution
889 Views
GordyCarlson
NXP Employee
NXP Employee

The Kinetis Errata for 3N96B mask set has this erratta.......

--------------------------------------------------------

e5952: SMC: Wakeup via the LLWU from LLS/VLLS to RUN to VLPR incorrectly

triggers an immediate wakeup from the next low power mode entry

Errata type: Errata

Description: Entering VLPR immediately after an LLWU wakeup event from LLS/VLLS, will cause any

subsequent entry into LLS/VLLS to fail if entry into VLPR mode occurs before clearing the

pending LLWU interrupt.

Workaround: After an LLWU wakeup event from LLS/VLLS, the user must clear the LLWU interrupt prior to

entering VLPR mode.

-------------------------------------------------------

Does this errata also affect wakeup/re-entry into VLLS2 after being in VLPR?  Thanks in advance for any clarification provided.

Gordy

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
513 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Gordon

Yes, please also pay attention workaround. Please add clear LLWU interrupt opreation before enter VLPR mode. Thanks.

Best Regards

Paul

View solution in original post

0 Kudos
Reply
1 Reply
514 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Gordon

Yes, please also pay attention workaround. Please add clear LLWU interrupt opreation before enter VLPR mode. Thanks.

Best Regards

Paul

0 Kudos
Reply