Kinetis K53 board support in MQX v4.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K53 board support in MQX v4.2

ソリューションへジャンプ
1,877件の閲覧回数
kfranz
Contributor III

Is there an MQX 4.2 board support package for the K53 like what is available for the K60, K64, K65, etc.? We are using the IAR EWARM compiler tools. If so, how do I download it?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,860件の閲覧回数
kfranz
Contributor III

Thank you for the help.

I will contact NXP technical support to get the BSP.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,868件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @kfranz ;

 

From what I can see, MQX 4.2 package supports twrk53n512.

danielchen_0-1642686612913.png

Now the latest MQX version is MQX v5.  please refer to below link for more details

https://www.nxp.com/design/software/embedded-software/mqx-software-solutions/mqx-v5-software-solutio...

There is no download link for legacy MQX 4.2.  If you need it,  I would suggest you contact with NXP technical support through a ticket.

 

Regards

Daniel

0 件の賞賛
返信
1,861件の閲覧回数
kfranz
Contributor III

Thank you for the help.

I will contact NXP technical support to get the BSP.

0 件の賞賛
返信