Kinetis K53 board support in MQX v4.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K53 board support in MQX v4.2

Jump to solution
1,214 Views
kfranz
Contributor III

Is there an MQX 4.2 board support package for the K53 like what is available for the K60, K64, K65, etc.? We are using the IAR EWARM compiler tools. If so, how do I download it?

Labels (1)
0 Kudos
Reply
1 Solution
1,197 Views
kfranz
Contributor III

Thank you for the help.

I will contact NXP technical support to get the BSP.

View solution in original post

0 Kudos
Reply
2 Replies
1,205 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @kfranz ;

 

From what I can see, MQX 4.2 package supports twrk53n512.

danielchen_0-1642686612913.png

Now the latest MQX version is MQX v5.  please refer to below link for more details

https://www.nxp.com/design/software/embedded-software/mqx-software-solutions/mqx-v5-software-solutio...

There is no download link for legacy MQX 4.2.  If you need it,  I would suggest you contact with NXP technical support through a ticket.

 

Regards

Daniel

0 Kudos
Reply
1,198 Views
kfranz
Contributor III

Thank you for the help.

I will contact NXP technical support to get the BSP.

0 Kudos
Reply