We are planning a new platform for future products. The Kinetis K22 with M4 core has worked well for us so far, but we need a few more peripherals with high-speed USB being a main requirement. Though we may need graphical LCDs at some point, most of our products will not, so the K7x would not make sense. I narrowed the Kinetis family list down to the K28 as FlexIO is an option for a future LCD or really just about any peripheral that we aren't currently planning for, which I believe is the purpose of FlexIO!
For a technology demo, I'm planning to purchase the FRDM-K28F board and connect a touch LCD which I read somewhere is possible.
1) Is there a recommended touch-LCD that will work with the FRDM-K28F (please provide a link)?
2) Is there example/demo code for making the LCD work with the FRDM-K28F using FlexIO?
Hello,
Answer to your questions: Does it a MUST with a touch-LCD panel? I am afraid we only provide a Graphical LCD. See an application note here: https://www.nxp.com/docs/en/application-note/AN5280.pdf